Technical FAQs

Ask a Question

Addition of Data Manager tool for Vijeo Designer version 4.5.1

Goals and Symptoms

Addition of Standalone Data Manager tool for Vijeo Designer version 4.5.1

Causes and Fixes

Data Manager is a graphical user interface for managing a target machine's recipe files (.rcp), data logging files (.dat), alarm files (.csv), video files (.vmg or .avi), snapshot files (.jpeg), and project backup files (.vdz)
It is automatically installed while Vijeo Designer is installed.
It can be installed in standalone (Vijeo Designer must be uninstalled before), in order to manage (send/retrieve/convert/edit) data from XBTG/GT targets with Vijeo Designer Run Time version 4.5.1.

 

Attachments

(Removed File URL: 187303_1FCA/Data-Manager.exe)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/0a0b0c279f835e68c1257329002c0f73/fl_block_5/0.132C?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL187303 V1.0, Originally authored by DaBr on 07/31/2007, Last Edited by DaBr on 07/31/2007
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?