Technical FAQs

Ask a Question

How do you create a new network connection with TwidoSuite?

Goals and Symptoms

Step by step procedure on adding a new connection in the connection manager.

Causes and Fixes

First, you will need to go to your program and select debug mode to go on line. To add a new connection, you will need to select connection management located at the button of the screen.


Once selected, click on the add button for adding a connection.


Once add is selected, the default will come up as follows to add the connection





Enter the IP address and apply.



Once applied, the connection manager will show the new connection that was added.


NOTE: The Twido PLC family is obsolete and has been replaced by the M221 family.
Was this helpful?
What can we do to improve the information ?