Technical FAQs

Ask a Question

Can the 584 PLC support four Modbus Ports?

Yes , with the use of the NW-BM85C002. The 584 has only 2 Modbus Ports.To get four Modbus Ports you must connect the bridge to one of the Modbus ports and configure port 1 of the bridge as a Slave port. The remainng three ports of the bridge then need to be configured as Master ports. This will allow the 584 to support 4 Modbus Ports.


Legacy KB System (APS) Data: RESL1868 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?