Technical FAQs

Ask a Question

When ordering a Quantum power supply, does the connector have to be ordered separately ?

No, the connector is included with the power supply. However there is an optional IP 20 compliant connector available (140XTS00500), which needs to be ordered separately.

Legacy KB System (APS) Data: RESL1863 V5.0, Originally authored by RiVe on 03/05/2008, Last Edited by DaSo on 10/08/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?