Technical FAQs

Ask a Question

Is SQL Data Manipulation Language (DML) supported in the Free SQL Request window of the FactoryCast HMI Database service?

The Free SQL Request window can not process SQL Data Manipulation Language (DML) commands when using executive versions 1.2 or 1.1. This new functionality will be added in FactoryCastHMI 1.3. Currently, the Free SQL Request window is designed to send basic administration of database SQL commands. The Free SQL Request window can not be used to read and write to a Database table.


Legacy KB System (APS) Data: RESL186037 V1.0, Originally authored by DaSo on 07/02/2007, Last Edited by DaSo on 07/02/2007
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?