Technical FAQs

Ask a Question

Can the Advantys STB DeviceNet NIM be used as a standalone bridge to Modbus ?

No. It cannot be used in this fashion. The minimum configuration for an Advantys STB island would be to have one PDT and one IO module. The suggestion is to use a Basic PDT and IO module to keep cost down. Then using the Advantys Configuration Software, these modules would have to be added to the configuration as well as HMI to PLC and PLC to HMI words configured in the NIM.


Legacy KB System (APS) Data: RESL184919 V1.0, Originally authored by DaSo on 07/03/2008, Last Edited by DaSo on 07/03/2008
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?