Technical FAQs

Ask a Question

What is the 24 Vdc amp rating on the Compact Twido's?

The 24 Vdc amp rating on the Compact Twido's is 400 mA for the 40DRF and 250 mA on all other Compact Twido's.


Legacy KB System (APS) Data: RESL184366 V3.0, Originally authored by DiSa on 06/11/2007, Last Edited by BrWa on 02/09/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?