Technical FAQs

Ask a Question

What is the maximum distance between two nodes in a Momentum Ibus or Interbus-S network?

The maximum distance between nodes are:
1. Shielded twisted pair is 400 Meters
2. LWL HCS fiber (200/230 um) is 300 Meters.
3. LWL Polymer fiber (980/1000 um) is 50 Meters.

Note: In a fiber network, the minimum distance between nodes are 1 meter.
There is no minimum distance between nodes on a twisted pair network.


Legacy KB System (APS) Data: RESL1843 V1.0, Originally authored by on , Last Edited by on
Related ranges: INTERBUS
Was this helpful?
What can we do to improve the information ?