Technical FAQs

Ask a Question

What are the differences between the Momentum 170AMM09000 and 170AMM09001 modules?

Both Momentum modules have 4 analog inputs and 2 analog outputs along with 4 discrete inputs and 2 discrete outputs.
The difference is the operating voltage and discrete In/Out voltage.
170AMM09000 = 24vDC
170AMM09001 = 12vDC

Was this helpful?
What can we do to improve the information ?