Technical FAQs

Ask a Question

How can I correct error '2007 - Invalid Band collection Index' error in ProWORX 32?

To correct this error, delete the layout.acf file which is found in the \proworx\32 folder. It will be recreated when ProWORX 32 is launched.


Legacy KB System (APS) Data: RESL184052 V1.0, Originally authored by DaSo on 05/15/2007, Last Edited by DaSo on 05/15/2007
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?