Technical FAQs

Ask a Question

Internet Explorer closes when the web page launches Java applet on ETZ510

Goals and Symptoms

Internet Explorer closes when the web page launches Java applet on ETZ510

Facts and Changes

TSXETZ510 Exec Firmware version 1.8

Causes and Fixes

The Internet Explorer window gets closed when a web page for a 'TSXETZ510' Ethernet module is
opened and the web page contains a Java applet.

This problem will occur on a TSXETZ510 module that has Exec Firmware version 1.8 and above.

The reason is becasue the PC does not have the 'Java Runtime Environment version 1.6.0' from 'Sun
Microsystems' installed or the option is not selected in the Internet Explorer 'Advanced' settings. .

If the 'Java Runtime Environment version 1.6.0' from 'Sun Microsystems' is not installed, download
it from 'http://java.com/en/' and install it.

  • Open Internet Explorer
  • Click on 'Tools\Internet Options'

 
  • Click on the 'Advanced' tab in the 'Internet Options' window.

 
  • Scroll down and locate the line for Java(Sun)
  • Click on the checkbox next to the item labeled 'Use JRE 1.6.0 for (applet ).... ' to select it.
  • Click on the 'Apply' button in the 'Internet Options' window.
  • Click on the 'OK' button in the 'Internet Options' window.
  • Close Internet Explorer and restart it.

 

Legacy KB System (APS) Data: RESL184045 V1.0, Originally authored by AlCh on 05/18/2007, Last Edited by AlCh on 05/18/2007
Related ranges: Modicon TSX Micro ETZ - TR
Was this helpful?
What can we do to improve the information ?