Technical FAQs

Ask a Question

Are there different types of Unity Application Generator (UAG)?

Commercially, two types of Unity Application Generator (UAG) software licenses are available.
- UAG
- UAG for the SE Alliance (SI)

UAG for the SE Alliance (SI) is exclusively available for certified Alliance Partners. All other parties are obliged to use the standard UAG package.

Both versions are functionally equivalent and support the PLC application generation for Unity Pro (Quantum, Premium, M340).
For the SCADA, the direct integration with application generation for Vijeo Citect and generation of additional HMI systems through customized XML files ( XSL style sheets).

Was this helpful?
What can we do to improve the information ?