Technical FAQs

Ask a Question

How to change the HTTP user name and password on the FactoryCast 140NOE77111 module.

Goals and Symptoms

How to change the HTTP user name and password on the FactoryCast 140NOE77111 module.

Causes and Fixes


Launch the FactoryCast Configurator tool



Open the File tab and select New Configuration



Under the Password tab change User Name and Password
Hit OK



Open the Transfer tab and select Security File



Insert the IP address of the FactoryCast NOE77111
Hit OK



When transfer process is complete recycle power to the NOE771 module by re-seating it



Launch IE and try the new User Name and Password


Legacy KB System (APS) Data: RESL183877 V1.0, Originally authored by MiMe on 04/27/2007, Last Edited by MiMe on 04/27/2007
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?