Technical FAQs

Ask a Question

What is the maximum number of variables that Vijeo Designer V4.5 can support?

Vijeo Designer V4.5 supports a maximum of 8000 variables.


Legacy KB System (APS) Data: RESL183864 V1.0, Originally authored by MiMe on 04/27/2007, Last Edited by MiMe on 04/27/2007
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?