Technical FAQs

Ask a Question

Why the 'Delete' key does not always work in the Logic window.

Goals and Symptoms

Why the 'Delete' key does not always work in the 'Logic' window.

Facts and Changes

All versions of 'ProWORX 32'

Causes and Fixes

If the blue logic cursor is on a an element after going to another network and you click on the 'Delete'
key on the keyboard, the element does not get deleted. This will occur because the mouse focus is not
on the logic element. To resolve the problem, you need to click on the element before hitting the 'Delete'
key on the keyboard.




If the above proceudre does not resolve the problem, check to see if the 'Use Insert /Delete Keys Menus'
option' in the Logic Properties window is selected, which causes the element to not get deleted immediately
and pops up a selection menu instead.




When the selection menu appears, you will need to select 'Element' before the element can get deleted.


.
.


Legacy KB System (APS) Data: RESL183827 V2.0, Originally authored by AlCh on 04/24/2007, Last Edited by AlCh on 04/26/2007
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?