Technical FAQs

Ask a Question

Do Cablefast cables have a maximum length?

Cablefast connection cables should not be longer than 15'. Cables over 15' in length are not supported.


Legacy KB System (APS) Data: RESL183825 V1.0, Originally authored by DaSo on 04/24/2007, Last Edited by DaSo on 04/24/2007
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?