Technical FAQs

Ask a Question

Is there a DIN rail standard for Momentum PRODUCTS?

The DIN rail standard is 35 mm (1.38 in) width. There are two depth sizes of DIN rail that can be used for mounting
Momentum IO bases, 7.5 mm (0.3 in) and 15 mm (0.6 in).

Was this helpful?
What can we do to improve the information ?