Technical FAQs

Ask a Question

Why am I getting an error that says "the hardware ID is (100) 03BF" when trying to load an executive into a Momentum CPU using Concept ?

This error will appear if bridge mode has been selected in the exec loader utility, deselect it and the Momentum CPU hardware ID should be identified successfully.

Was this helpful?
What can we do to improve the information ?