Technical FAQs

Ask a Question

Is Vijeo Citect V6.1 available only in English?

Vijeo Citect V6.1 is available in the the following languages: English, French, German, Chinese, Japanese, Korean.
The installer automatically detects the language of the operating system on the machine, and installs the same language if available. If the OS is in an unavailable language, English is installed as the default language.


Legacy KB System (APS) Data: RESL183437 V1.0, Originally authored by MiMe on 04/10/2007, Last Edited by MiMe on 04/10/2007
Related ranges: Other HMI
Was this helpful?
What can we do to improve the information ?