Technical FAQs

Ask a Question

How do I enable the "Merge Data Logging into Single file" option in Vijeo-Designer Data Manager V4.5?

In Data Manager, the "Merge Data Logging into single file" option is greyed out if the "Build Tree" option is checked in the Data Manager Options dialog box. To enable the "Merge Data Logging into single file" option, you need to uncheck the "Build Tree" option


.


Legacy KB System (APS) Data: RESL183436 V1.0, Originally authored by MiMe on 04/10/2007, Last Edited by MiMe on 04/10/2007
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?