Technical FAQs

Ask a Question

Can the password protection for my Twido application be removed?

Yes. In order to remove the password, you will need to know the old password. To remove password protection from an application, you
will need to do the following:

 

1.
Open the application that has been password protected using the current password.
2.
Select Program - Change Password from the main menu.
3.
Type the current password in Enter Old Password. Do not enter a password in "New Password " field, tab through the other boxes.
4.
Select OK to close the box.

The application must be saved to remove password protection.

Note: The Twido line has been obsoleted 12/31/2016 and has been replaced with the M221 line.
Was this helpful?
What can we do to improve the information ?