Technical FAQs

Ask a Question

What is the maximum loop impedance for the following Advantys STB analog output modules STBACO1210, STBACO0220, and STBACO1225?

The maximum load impedance is 500 ohms.


Legacy KB System (APS) Data: RESL183378 V1.0, Originally authored by DaSo on 04/11/2007, Last Edited by DaSo on 04/11/2007
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?