Technical FAQs

Ask a Question

What could cause the error "Unknown Modbus Exception code Error ID: OL9-21504" when trying to connect to the Concept IEC simulator?

One possible explanation for this error is a conflict between Concept and the v6.0 Ethernet MBX driver. Uninstalling the v6.0 Ethernet MBX driver and rebooting the PC will correct the issue.


Legacy KB System (APS) Data: RESL182599 V1.0, Originally authored by MiMe on 03/13/2007, Last Edited by MiMe on 03/13/2007
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?