Technical FAQs

Ask a Question

Setting up an IP address on a OTB1E0DM9LP version 1.4 module Using the Advantys Configuration Software ver 2.5

Goals and Symptoms

Setting up an IP address on a OTB1E0DM9LP version 1.4 module Using the Advantys Configuration Software ver 2.5

Facts and Changes

This resolution is valid for an older version of the Advantys software (version 2.5).
The current version of the Advantys software is 4.5 and has a different method for uploading the IP parameters.

Causes and Fixes

Setting up an IP address on a OTB1E0DM9LP version 1.4 module Using the Advantys Configuration Software ver 2.5



Launch Advantys Configuration Software and select OTB.



Select Create a new Island. Name the new Island.



Select the OTB module from the list and drop it onto the rail.



Select the Upload Configuration button.



Enter the last two values of the OTBs MAC address and you will notice that the last two octets of the default IP address will automatically fill in. (Write the full default IP address down then press the Upload IP parameters button.)



Power off the OTB.
Change the right rotary wheel position to IP.
Connect a RJ45 crossover patch cable from your computer to the OTB.
Power on the OTB and after a few min. the amber STAT light on the OTB will flash 6 times.
Press the OK button.



Note: You should try to ping the default IP address at this point which will check youre cabling to the OTB. The easiest way to do this is by changing the IP address on your computer to match the OTB's default IP address with the last octet off by one value.



Enter all the correct IP information and press the Upload button while using the default IP address. (If no gateway is available leave empty and the software will use the OTBs IP address)


Power off the OTB.
Change both rotary wheel position to something other then IP or BOOTP.
Change the IP address to your computer to its normal address.
Power on the OTB and the amber STAT light will be on solid, now make sure you can ping the OTB with its new IP address.


Legacy KB System (APS) Data: RESL182593 V2.0, Originally authored by MiMe on 03/13/2007, Last Edited by MiMe on 09/17/2009
Related ranges: Advantys OTB
Was this helpful?
What can we do to improve the information ?