Technical FAQs

Ask a Question

Does Proworx32 support the 584 controller?

ProWORX 32 version 2.0 will convert a 584 project but will not communicate to a 584 PLC.
Version 2.1 will upload a 584 project, import and download a 584 project the user cannot create a 584 project.
The 584 PLC is not a choice in the PLC pick list when creating a new project with version 2.1.


Legacy KB System (APS) Data: RESL182568 V1.0, Originally authored by DaSo on 03/13/2007, Last Edited by DaSo on 03/13/2007
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?