Technical FAQs

Ask a Question

Vijeo Look 2.6: use of OFS 3.31

Goals and Symptoms


After the OFS 3.31 update, OFS Configuration Tool is no longer available from the Vijeo Look Tools Menu.

Facts and Changes


Vijeo Look 2.6 has not been qualified with OFS 3.31 release.

However a short testing phase with this package showed no error.

Except for the Tool Menu, that does not launch the release 3.31 of the OFS Configuration Tool.

Causes and Fixes


OFS 3.31 does not install the registry key:

HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\App Paths\OFSconf.exe

If this registry key is manually added using REGEDIT Windows tool, and filled with the actual and complete path to OFSConf.exe, the problem is fixed.


Legacy KB System (APS) Data: RESL182555 V1.0, Originally authored by PaBo on 03/09/2007, Last Edited by PaBo on 03/09/2007
Related ranges: Vijeo Look
Was this helpful?
What can we do to improve the information ?