Technical FAQs

Ask a Question

Different behaviour of latched coils in Modsoft and Concept

Goals and Symptoms


This resolution describes a different behaviour of latched coils in Modsoft and Concept

Causes and Fixes

Under Modsoft, after uploading and then downloading the StateRAM, the values of the latched coils
appear as they were during the Upload.

Under Concept, after uploading and then downloading the StateRAM, all values of the latched coils
are resetted. The Concept Upload/Download function doesn't care about the usage of the 0x/1x values
because it has no information whether a 0x register is used as a latched coil.


Legacy KB System (APS) Data: RESL182545 V1.0, Originally authored by EcMO on 03/09/2007, Last Edited by EcMO on 03/09/2007
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?