Technical FAQs

Ask a Question

What is the maximum number of PLC's supported by VijeoLook acting as a SCADA system?

The maximum number of PLC systems supported by VijeoLook as a SCADA is 5.


Legacy KB System (APS) Data: RESL182313 V1.0, Originally authored by DaSo on 02/22/2007, Last Edited by DaSo on 02/22/2007
Related ranges: Vijeo Look
Was this helpful?
What can we do to improve the information ?