Technical FAQs

Ask a Question

What are the I/O limitations on the M340 CANopen processors?

The M340 CANopen master supports a maximum of 63 I/O modules with a maximum I/O limit of 512 digital and 1024 Analog I/O points.


Legacy KB System (APS) Data: RESL182114 V1.0, Originally authored by TVe on 02/13/2007, Last Edited by TVe on 02/13/2007
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?