Technical FAQs

Ask a Question

What is the IP protection class for the BPH motor power and feedback cables?

The only available IP protection for the power and feedback cables is IP 67.


Legacy KB System (APS) Data: RESL182113 V1.0, Originally authored by TVe on 02/13/2007, Last Edited by TVe on 02/13/2007
Related ranges: Lexium 17D
Was this helpful?
What can we do to improve the information ?