Technical FAQs

Ask a Question

How do I add a new network using the ProWORX Plus software?

A network can be added before or after the current network.
To insert a new network:
1- Press the "INSERT" key on your keyboard. The Insert menu bar will appear on the screen.
2- Press "F6" to insert a new blank network immediately before the current network displayed or press "F5" to insert a new blank network after the current network displayed.


Legacy KB System (APS) Data: RESL182019 V1.0, Originally authored by RoAl on 02/08/2007, Last Edited by RoAl on 02/08/2007
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?