Technical FAQs

Ask a Question

Which communication ports are supported in the 8010SFW30 software for SyMax Micro 1 controllers?

The SFW30 interface port can only be configured as "COM1" or "COM2". Other ports, COM3, COM4, etc... are not acceptable port configurations even though the physical ports may exist.


Legacy KB System (APS) Data: RESL182014 V1.0, Originally authored by RoAl on 02/07/2007, Last Edited by RoAl on 02/07/2007
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?