Technical FAQs

Ask a Question

Declaration of conformity for ASISSLC1 and for ASISAFEMON2B

Goals and Symptoms

Declaration of conformity for ASISSLC1 and for ASISAFEMON2B

Facts and Changes

Declaration of conformity
AS-interface "safety at work" components
ASISAFEMON1/2(B) monitors
ASISSL* safety interfaces

Causes and Fixes

Find attached all the 3 declarations of conformity existing in 2007, for all the safety interfaces & safety monitors (2 versions), delivered with our PRODUCTS in the package. They refer to the machinery directive and we precise the standards of reference inside

Attachments

(Removed File URL: 181748_D956/declaration_CE_ASISAFEMON_ASISSx.ZIP)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/fa88ae5afbb0dd21c125726e00582955/fl_block_5/0.137C?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL181748 V1.0, Originally authored by on , Last Edited by JeLe on 01/25/2007
Related ranges: AS-Interface safety at work
Was this helpful?
What can we do to improve the information ?