Technical FAQs

Ask a Question

'Advantys Configuration Software version 2.5 returns 'Error 35603' when trying to open an older application

Goals and Symptoms

'Advantys Configuration Software version 2.5 returns 'Error 35603' when trying to open an application
that was created with 'Advantys Configuration Software version 2.2'.

Facts and Changes

Advantys Configuration Software version 2.5

Causes and Fixes

'Advantys Configuration Software version 2.5 returns 'Error 35603' when trying to open an application
that was created with 'Advantys Configuration Software version 2.2'.

The problem only happens on a PC that is running the French language version of the 'Microsoft
Windows 2000' operating system.



We expect a patch to be available for fixing this problem sometime near the end of Q1/07.


Legacy KB System (APS) Data: RESL181738 V1.0, Originally authored by on , Last Edited by AlCh on 01/26/2007
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?