Technical FAQs

Ask a Question

Where is the 'ProWORX 32 Server' project backup stored

Goals and Symptoms

Where is the Server project backup stored

Causes and Fixes

By default, the server backups are stored in the folder C:\ProWORX\32\Server\Projects\ProjectName~BAK


The filename for the back up is in the form of ' 000001~ProjectName~Date~...'


It will always be stored be in a subfolder under the defined Server projects folder.

i.e., if the server project folder is defined as

C:PW32\Server\Projects\

The project backup from the server will be stored in the subfolder named

C:PW32\Server\Projects\ProjectName~BAK


Legacy KB System (APS) Data: RESL181677 V1.0, Originally authored by on , Last Edited by AlCh on 02/20/2007
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?