Technical FAQs

Ask a Question

What causes an 'out of string space' error when importing a project into ProWORX 32?

This error message will be displayed if the Modsoft project being imported does not have any networks. Add an empty network and the project should import.


Legacy KB System (APS) Data: RESL181453 V1.0, Originally authored by DaSo on 01/06/2007, Last Edited by DaSo on 01/06/2007
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?