Technical FAQs

Ask a Question

What is included in the TSXISPY121 Premium Weighing indicator package?

The Premium Weighing indicator package (TSXISPY121) includes :
· 1 weighing module TSXISPY101
· 1 compact display unit TSXXBTN410
· 1 3-meter cable to connect the weighing module to the display unit TSXCPY030


Legacy KB System (APS) Data: RESL181282 V1.0, Originally authored by GeMc on 12/28/2006, Last Edited by GeMc on 12/28/2006
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?