Technical FAQs

Ask a Question

Can you order the Twido I/O module TWDDMM24DRF with screw terminals?

No, It is only offered with the non-removable spring terminals.


Legacy KB System (APS) Data: RESL181265 V1.0, Originally authored by GeMc on 12/28/2006, Last Edited by GeMc on 12/28/2006
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?