Technical FAQs

Ask a Question

What are the part numbers to the Terminal Blocks for the M340 I/O cards?

The Terminal blocks are :
BMXFTB2000 Screw terminal strip (20 points)
BMXFTB2010 Square washer terminal strip (20 points)
BMXFTB2020 Spring terminal strip (20 points)


Legacy KB System (APS) Data: RESL180825 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?