Technical FAQs

Ask a Question

What is the part number to the USB to Modbus Plus converter?

The part number for the USB to Modbus Plus converter is TSXCUSBMBP.


Legacy KB System (APS) Data: RESL180824 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?