Technical FAQs

Ask a Question

Are the 3rd party protocols included in XBTL1000 V4.5?

Yes. The 3rd Protocols are included in both the lite and full packages of XBTL1000 V4.5.


Legacy KB System (APS) Data: RESL180819 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: XBT L1000
Was this helpful?
What can we do to improve the information ?