Technical FAQs

Ask a Question

What are the Minimum System Requirements to run XBTL1000 V4.5?

The Minimum System Requirements for XBTL1000 V4.5 are:
PC Pentium II 350 MHz
Minimum 4x CD-ROM drive
Windows 98, 2000, or XP
64 MB RAM (128 MB RAM recommended for WIN 2000/XP
30 MB Hard Drive space
SVGA video or higher
Mouse or compatible pointer system


Legacy KB System (APS) Data: RESL180818 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: XBT L1000
Was this helpful?
What can we do to improve the information ?