Technical FAQs

Ask a Question

What are the new 3rd party Protocols for the XBTN and XBTR available in XBTL1000 V4.5?

The new 3rd party protocols for XBTN and XBTR terminals added in V4.5 of XBTL1000 are:
Siemens s7-200: PPI
Rockwell automation Micrologix: DF1
Rockwell automation Micrologix: DH485
Omron CPM Sysmacway
Mitsubishi FX0N/FX1N/FX1S/FX2N/FX2NC/FX FX2C: Melsec


Legacy KB System (APS) Data: RESL180816 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: XBT L1000
Was this helpful?
What can we do to improve the information ?