Technical FAQs

Ask a Question

What are the part numbers to the terminal block and cables with HE10 connectors for the M340 I/O?

The part numbers to the terminal block & cables with HE10 connectors for the M340 I/O are:
BMXFCCxx1 1 FCN to 1 HE10 for direct wiring with Telefast 2 system.
BMXFCCxx3 1 FCN to 2 HE10 for direct wiring with Telefast 2 system.
where xx = 05 (0.5 meter), 10 (1.0 meter), 30 (3.0 meters), 50 (5.0 meters), or 100 (10.0 meters)


Legacy KB System (APS) Data: RESL180813 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?