Technical FAQs

Ask a Question

What is the RTD slope specifications of the IEC and US/JIS modes of the Advantys STB ART 0200?

The STBART02000 can handle IEC PT100 RTD with a European alpha of 0.00385 ohms/ohm/degC and US/JIS PT100 RTD with a American alpha of 0.00392 ohms/ohm/degC.
The corresponding temperature ranges are -200 to 850 DegC for IEC and -100 to 450 DegC for US.

Was this helpful?
What can we do to improve the information ?