Technical FAQs

Ask a Question

What are the differences between the small (TLXCDSUOFS36) and large (TLXCDLUOFS36) OFS V3.6 packages?

The small package of OFS (TLXCDSUOFS36) has the same features of the large package (TLXCDLUOFS36) except for the following restrictions:
1) The size of the application (Number of items managed by the server) is limited to 1000 tags.
2) The OPC XML protocol and Web interface are not available.


Legacy KB System (APS) Data: RESL180801 V1.0, Originally authored by GeMc on 12/05/2006, Last Edited by GeMc on 12/05/2006
Related ranges: OPC/OPP/VIC
Was this helpful?
What can we do to improve the information ?