Technical FAQs

Ask a Question

What does error message 'Error ID MN-106 -Illegal file extension for the database file' mean when opening a Concept project?

This error usually means that the path name is too long. It exceeds 32 characters.


Legacy KB System (APS) Data: RESL180630 V1.0, Originally authored by DaSo on 02/17/2009, Last Edited by DaSo on 02/17/2009
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?