Technical FAQs

Ask a Question

Are the TCSESM managed switches compliant with LLoyds Registry certification?

The TCSESM managed switches are not compliant with LLoyds Register certification. LLoyds Register certification is not part of the normal certification process. There are no current plans to have them added to the certification process.
The certification that the TCSESM managed switches have is the CE certification.

Was this helpful?
What can we do to improve the information ?