Technical FAQs

Ask a Question

What replaces the 140EDK77100 ?

The 140EDK77100 was an Ethernet Development Kit. The function of the ethernet development kit has been included into the firmware of the 140NOE77111. The firmware along with the downloadable Factory Cast Configuration files make up the SDK ( software development kit ) component of the module.


Legacy KB System (APS) Data: RESL180350 V1.0, Originally authored by DaSo on 10/17/2006, Last Edited by DaSo on 10/17/2006
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?