Technical FAQs

Ask a Question

TSXETG100 may exhibit intermittent communications when using the RS485 or RS232 serial ports.

Cause: Faulty component causing incorrect value of inductance.
Origin: Supplier: One lot of components, identifiable by date code, is in non-conformance with the components specifications.
This issue applies only to units manufactured between the dates of 06/15/2006 (June 15, 2006) through 09/15/2006 (September 15, 2006).
The majority of the affected units have been contained to the factory, the number of impacted units is limited, and the severity level of the issue is low. The manufacture date is printed on the side of the unit.

Resolution: Any units that meet the date code range and exhibit the stated conditions should be exchanged.


Legacy KB System (APS) Data: RESL180190 V1.0, Originally authored by DaSo on 10/23/2006, Last Edited by DaSo on 10/23/2006
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?